imx-weim

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx-weim

2,003 次查看
niklasmolin
Senior Contributor I

Hi.

I'm wonder if someone has an example how to use the imx-weim driver?

Thanks,

Niklas

标签 (2)
0 项奖励
回复
1 回复

1,311 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

"weim" is usually supported through parallel NOR flash driver,

which present in i.MX Auto boards, for example below i.MX6 Sabre Auto

links. i.MX_6Dual6Quad_Linux_Reference_Manual.pdf describes weim nor driver.

L3.0.35_4.1.0_LINUX_DOCS

RDIMX6SABREAUTO: SABRE for Automotive Infotainment Based on the i.MX 6 Series: SABRE for Automotive ...

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复