imx-weim

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-weim

2,588 Views
niklasmolin
Senior Contributor I

Hi.

I'm wonder if someone has an example how to use the imx-weim driver?

Thanks,

Niklas

Labels (2)
0 Kudos
Reply
1 Reply

1,896 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

"weim" is usually supported through parallel NOR flash driver,

which present in i.MX Auto boards, for example below i.MX6 Sabre Auto

links. i.MX_6Dual6Quad_Linux_Reference_Manual.pdf describes weim nor driver.

L3.0.35_4.1.0_LINUX_DOCS

RDIMX6SABREAUTO: SABRE for Automotive Infotainment Based on the i.MX 6 Series: SABRE for Automotive ...

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply