iMX8QM DDR Stress Test Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8QM DDR Stress Test Issue

3,790 次查看
prashanthkumar
Contributor II

Hi,

We are working on i.MX8QM custom board with 8GB LPDDR4 supported DDR.

We used latest DDR stress tool(ER14) and RPA tool (v19 and v20) from the below NXP site.

i.MX 8/8X Family DDR Tools Release  

But is hanging in the middle of the 8GB LPDDR4 stress test. The same is working fine for old RPA tool(v17) with old Stress tool(ER8). Is there any latest RPA tool for LPDDR4 supported iMX8QM board?

The hanged Stress tool image is attached for your reference.

Best Regards,

Prashanth Kumar K

0 项奖励
回复
2 回复数

3,587 次查看
vinothkumars
Senior Contributor IV

Hi @prashanthkumar ,

 

Will you please share the old RPA tool(v17) with old Stress tool(ER8)

Regards,
Vinothkumar Sekar
标记 (1)
0 项奖励
回复

3,685 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth 

>Is there any latest RPA tool for LPDDR4 supported iMX8QM board?

please look at i.MX 8/8X Family DDR Tools Release  

>The same is working fine for old RPA tool(v17) with old Stress tool(ER8).

one can look at latest RPA tool, Tab "Revision History" for chnages since v17.

>But is hanging in the middle of the 8GB LPDDR4 stress test.

one can try to tweak drive strength/odt settings (details were sent via mail).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复