iMX8QM DDR Stress Test Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QM DDR Stress Test Issue

3,802 Views
prashanthkumar
Contributor II

Hi,

We are working on i.MX8QM custom board with 8GB LPDDR4 supported DDR.

We used latest DDR stress tool(ER14) and RPA tool (v19 and v20) from the below NXP site.

i.MX 8/8X Family DDR Tools Release  

But is hanging in the middle of the 8GB LPDDR4 stress test. The same is working fine for old RPA tool(v17) with old Stress tool(ER8). Is there any latest RPA tool for LPDDR4 supported iMX8QM board?

The hanged Stress tool image is attached for your reference.

Best Regards,

Prashanth Kumar K

0 Kudos
Reply
2 Replies

3,599 Views
vinothkumars
Senior Contributor IV

Hi @prashanthkumar ,

 

Will you please share the old RPA tool(v17) with old Stress tool(ER8)

Regards,
Vinothkumar Sekar
Tags (1)
0 Kudos
Reply

3,697 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth 

>Is there any latest RPA tool for LPDDR4 supported iMX8QM board?

please look at i.MX 8/8X Family DDR Tools Release  

>The same is working fine for old RPA tool(v17) with old Stress tool(ER8).

one can look at latest RPA tool, Tab "Revision History" for chnages since v17.

>But is hanging in the middle of the 8GB LPDDR4 stress test.

one can try to tweak drive strength/odt settings (details were sent via mail).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply