Thunderbolt compatible with iMX8MPlus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Thunderbolt compatible with iMX8MPlus

ソリューションへジャンプ
2,349件の閲覧回数
GuiDas
Contributor II

Hello,

 

I am currently working on the iMX8MPlus and I would like to know if the USB 3.0 connected to an USB C connector  could be compatible with the Thunderbolt protocol ?

 

Thank you in advance,

 

Guilhem

0 件の賞賛
返信
1 解決策
2,344件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello GuiDas,

It could be compatible but the transfer going to be as usb 3.0.

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,345件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello GuiDas,

It could be compatible but the transfer going to be as usb 3.0.

Regards

 

0 件の賞賛
返信
2,334件の閲覧回数
GuiDas
Contributor II

Thank you for you answer, I just need a precision,when you say "transfer going to be as usb 3.0", you mean the data rat ?

I have another question following your answer, do I need to implement something special in hardware/software in order to have the thunderbolt ?

Thank you,

Guilhem

0 件の賞賛
返信
2,308件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi, yes i refer to data rate and not change from I.MX side.

regards

 

0 件の賞賛
返信