iMX8MP wayland extended display mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8MP wayland extended display mode

2,090 次查看
zb2020
Contributor II

I'm using iMX8MP EVK with Yocto Kirkstone (wayland) platform to drive two displays (HDMI+LVDS0). The wayland runs in extended desktop mode. Both display interfaces are working, the wayland toolbar is visible on both displays.

How can I auto launch an application programmatically on the secondary display? The apps launched from command line always are displayed on the first display.



标签 (1)
0 项奖励
回复
6 回复数

2,042 次查看
zb2020
Contributor II

I'm using imx-yocto-L5.15.52_2.1.0.

0 项奖励
回复

2,022 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @zb2020 ,

I hope you're doing great. As far as I know, this feature is not supported with our BSP, but let me double check with our team to confirm this or if there is another way to achieve this.

Thank you.

Best regards,
Hector.

0 项奖励
回复

1,974 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @zb2020 ,

I hope you're doing well. I don't think this can be done with Wayland, but there may be some configurations in U-boot to allow this, I'll research this further.

Thank you.

Best regards,
Hector

0 项奖励
回复

2,058 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @zb2020 ,

I hope you're doing great. What BSP version are you using? Thank you.

Best regards,
Hector.

0 项奖励
回复

1,935 次查看
zb2020
Contributor II

I'm using imx-yocto-L5.15.52_2.1.0.

0 项奖励
回复

1,907 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @zb2020 ,

I hope you're doing great and sorry for the late response. After further review with our team we got to the conclusion that this wouldn't be possible through Wayland Weston or U-Boot. This las option can only define the default display for all applications and unfortunately can't be software specific. To achieve what you're trying to do, it must be done through the application's code (so it'd be app specific). Thank you.

Best regards,
Hector.

0 项奖励
回复