Hi.
How can I use LPUART4(ttyLP4) ?
I made the following changes and the device ttyLP4 is recognized.
However, there is an error in the console message and LPUART4 cannot be used.
Am I missing something or is it wrong?
environment
・Android-11.0.0_2.6.0
・MCIMX8QM-CPU + MCIMX8-8X-BB
changes
・init.rc (/device/nxp/imx8q/mek_8q)
- Added the following code before "on boot".
chmod 0777 /dev/ttyLP4
・imx8qm-ss-dma.dtsi (/vendor/nxp-opensource/kernel-imx/arch/arm64/boot/dts/freescale)
- Added the following code.
&lpuart4 {
compatible = "fsl,imx8qm-lpuart", "fsl,imx8qxp-lpuart";
};
・imx8qm-mek.dts (/vendor/nxp-opensource/kernel-imx/arch/arm64/boot/dts/freescale)
- added the following code.
&lpuart4 {
pinctrl-0 = <&pinctrl_lpuart4>;
status = "okay";
};
pinctrl_lpuart4: lpuart4grp {
fsl,pins = <
IMX8QM_M40_GPIO0_00_DMA_UART4_RX 0x06000020
IMX8QM_M40_GPIO0_01_DMA_UART4_TX 0x06000020
>;
};
boot msg
[ 0.674545] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.677943] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 55, base_baud = 5000000) is a FSL_LPUART
[ 1.932236] printk: console [ttyLP0] enabled
[ 1.937290] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 56, base_baud = 5000000) is a FSL_LPUART
[ 1.947052] imx8qm-pinctrl scu:pinctrl: pin_config_set op failed for pin 9
[ 1.953939] fsl-lpuart 5a0a0000.serial: Error applying setting, reverse things back
[ 1.961846] 5a0a0000.serial: ttyLP4 at MMIO 0x5a0a0010 (irq = 79, base_baud = 5000000) is a FSL_LPUART
Solved! Go to Solution.
Hello Sushi,
The root cause it that pin M40_GPIO0_00 and M40_GPIO0_01 are assigned to M core0 in scfw. When doing pin config, scfw will reject the request from Linux. Please check the variable pad_list in the below section of scfw.
To enable lpuart4 in imx8qm, you might need update the scfw as requirement and disable the uart function in M core0 demo.
regards
I have the same problem and cannot use LPUART4.
I hope NXP will resolve this issue as soon as possible.
The structure declaration in imx-scu.c (/ kernel_imx / drivers / firmware / imx) says "SCU uses 4 Tx and 4 Rx channels".
I think there are 0 to 4 channels, is that different?
Isn't it a total of 10 channels (5 Tx and 5 Rx channels)?
Is this related to this issue?
"SCU uses 4 Tx and 4 Rx channels"
I learned that this description refers to the MU in the SCU.
The MU has two processors, each with four registers.
There are 8 channels in total.
It is DMA that has 5 LPUARTs.
Please give me a reply...
I am checking the functions called at startup step by step.
After the "... failed for pin9",
In the pinctrl_commit_state function of core.c(/kernel_imx/drivers/pinctrl), the return value "-13" is returned.
Moreover,
According to the description in imx-scu.c(/kernel_imx/drivers/firmware/imx), the meaning of "-13" is "EACCES".
In other words,
It turned out to be a "Permission error (no access)".
What causes this error?
Please tell me how to deal with it.
Hello Sushi,
The root cause it that pin M40_GPIO0_00 and M40_GPIO0_01 are assigned to M core0 in scfw. When doing pin config, scfw will reject the request from Linux. Please check the variable pad_list in the below section of scfw.
To enable lpuart4 in imx8qm, you might need update the scfw as requirement and disable the uart function in M core0 demo.
regards
Hi, @Bio_TICFSL
Your advice has solved this problem.
I checked pad_list in boad.c.
And I changed the following section(M core0 in scfw).
before: RM_RANGE (SC_P_M40_I2C0_SCL, SC_P_M40_GPIO0_01)
after: RM_RANGE (SC_P_M40_I2C0_SCL, SC_P_M40_I2C0_SDA)
I wrote the image built by replacing scfw_tcm.bin.
Now there are no startup errors and ttyLP4 can be used normally.
Thank you, I'm happy.
Hello ,I got some problem in the scfw with Android AutoMotive compile,can you describe the details of compile scfw and Android AutoMotive?I need your help
hello @EmptyObject_
I don't know much about SCFW compile.
but, I don't know your problem too. what's your problem?
do you have thread URL about it ?