iMX8MP ISP - How to disable WDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP ISP - How to disable WDR3

1,727 Views
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if there's a simple way to disable WDR3 feature without using vvext utility please ? My problem is that WDR3 is enabled by default when launching gstreamer and it makes the scene/images brighter but not natural (over-exposure).

Also, even-though I disabled it after first gst-launch (and it does keep it status as disabled), but second gst-launch would require a cycle of re-enable/re-disable to correctly disable it.

Thanks in advance and best regards,

Khang

0 Kudos
Reply
3 Replies

1,718 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the ISP Using V4L2 Interface User Guide,

joanxie_0-1656647026807.png

joanxie_1-1656647057048.png

maybe you can double check these control words to disable it

 

0 Kudos
Reply

1,714 Views
khang_letruong
Senior Contributor III

Hi @joanxie ,

Thanks for your reply. Do you mean that I could use the v4l2-ctl command to control this WDR3's parameters? If yes, could you give an example of the syntax, please ?

Thanks in advance and best regards,

Khang

 

0 Kudos
Reply

1,705 Views
artsiomstaliaro
Contributor IV

Example you can find in source code of vvext tool

0 Kudos
Reply