iMX8 boot kernel from micro-sd having SDIO WP enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 boot kernel from micro-sd having SDIO WP enabled

1,500 Views
Joomar
Contributor II

The boot from micro-sd having SDIO WP signal enabled hangs with error -30 "/dev/root: Can't open blockdev "

Why it is not possible to mount the root device with the write protection?

is there a work around? like enabling the "wp-gpios" after the boot?

0 Kudos
Reply
1 Reply

1,448 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel is protected so, the SD WP need to be non-write enable to work with it.

Regards

0 Kudos
Reply