iMX8 boot kernel from micro-sd having SDIO WP enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 boot kernel from micro-sd having SDIO WP enabled

1,492件の閲覧回数
Joomar
Contributor II

The boot from micro-sd having SDIO WP signal enabled hangs with error -30 "/dev/root: Can't open blockdev "

Why it is not possible to mount the root device with the write protection?

is there a work around? like enabling the "wp-gpios" after the boot?

ラベル(2)
0 件の賞賛
返信
1 返信

1,440件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel is protected so, the SD WP need to be non-write enable to work with it.

Regards

0 件の賞賛
返信