iMX8 RNDIS USB Reset issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 RNDIS USB Reset issue

2,526 Views
lyfsci
Contributor III

Hi Experts,

We tried to use the RNDIS mode device with iMX8 platform through USB port. The device is getting re-enumerated again and USB trace logs shows it that Reset is issued by USB host.

Please suggest method to debug the same.

0 Kudos
Reply
1 Reply

2,386 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lyf

one can try with usb unit tests

mxc_usb_test\test - imx-test - i.MX Driver Test Application Software 

for debugging, usb driver is described in Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply