ERR003739 Imprecise abort on the last data of a cache linefill may not be detected in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERR003739 Imprecise abort on the last data of a cache linefill may not be detected in i.MX6DQ.

565件の閲覧回数
keitanagashima
Senior Contributor I

Dear Victor,

>You can avoid this errata by using granularity not smaller than cache line.

Realistically I think that the errata can't avoid by customer side because it is not implemented in BSP(Android/Linux).

>I did not find errata 751470 in public Cortex-A9 errata list too.

>Perhaps it is some confidential errata.

OK. But, NXP published the errata.

The errata looks very important.

Please tell me the plan to fix this errata.

Best Regards,

Keita

0 件の賞賛
返信
1 返信

517件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  I've sent You some comments directly.

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信