iMX8 RNDIS USB Reset issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 RNDIS USB Reset issue

2,541件の閲覧回数
lyfsci
Contributor III

Hi Experts,

We tried to use the RNDIS mode device with iMX8 platform through USB port. The device is getting re-enumerated again and USB trace logs shows it that Reset is issued by USB host.

Please suggest method to debug the same.

ラベル(1)
0 件の賞賛
返信
1 返信

2,401件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lyf

one can try with usb unit tests

mxc_usb_test\test - imx-test - i.MX Driver Test Application Software 

for debugging, usb driver is described in Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信