iMX8 QuadMax ADB connection unreliable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 QuadMax ADB connection unreliable

Jump to solution
1,983 Views
mt_android
Contributor I

Hi,

I have android running iMX8 QuaMax board that connects to my laptop, however ADB connection is unreliable. When plugin usb, the device is shown by running adb devices, and I can use adb shell/push for a while, and then the device is offline. I need to reconnect usb cable to get the device back.

Is it a common issue? And how to fix it?

Thanks a lot. 

0 Kudos
Reply
1 Solution
1,977 Views
b36401
NXP Employee
NXP Employee

Possibly UART connection is weak and the connection drops by some glitch.
Please try to change cable, etc.

View solution in original post

0 Kudos
Reply
2 Replies
1,978 Views
b36401
NXP Employee
NXP Employee

Possibly UART connection is weak and the connection drops by some glitch.
Please try to change cable, etc.

0 Kudos
Reply
1,962 Views
mt_android
Contributor I

I changed the cable, and it is the samething. The ADB connection gets lost in several minutes after plugged in.

0 Kudos
Reply