iMX8 QuadMax ADB connection unreliable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8 QuadMax ADB connection unreliable

跳至解决方案
1,951 次查看
mt_android
Contributor I

Hi,

I have android running iMX8 QuaMax board that connects to my laptop, however ADB connection is unreliable. When plugin usb, the device is shown by running adb devices, and I can use adb shell/push for a while, and then the device is offline. I need to reconnect usb cable to get the device back.

Is it a common issue? And how to fix it?

Thanks a lot. 

0 项奖励
回复
1 解答
1,945 次查看
b36401
NXP Employee
NXP Employee

Possibly UART connection is weak and the connection drops by some glitch.
Please try to change cable, etc.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,946 次查看
b36401
NXP Employee
NXP Employee

Possibly UART connection is weak and the connection drops by some glitch.
Please try to change cable, etc.

0 项奖励
回复
1,930 次查看
mt_android
Contributor I

I changed the cable, and it is the samething. The ADB connection gets lost in several minutes after plugged in.

0 项奖励
回复