iMX8 QuadMax ADB connection unreliable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 QuadMax ADB connection unreliable

ソリューションへジャンプ
1,939件の閲覧回数
mt_android
Contributor I

Hi,

I have android running iMX8 QuaMax board that connects to my laptop, however ADB connection is unreliable. When plugin usb, the device is shown by running adb devices, and I can use adb shell/push for a while, and then the device is offline. I need to reconnect usb cable to get the device back.

Is it a common issue? And how to fix it?

Thanks a lot. 

ラベル(3)
0 件の賞賛
返信
1 解決策
1,933件の閲覧回数
b36401
NXP Employee
NXP Employee

Possibly UART connection is weak and the connection drops by some glitch.
Please try to change cable, etc.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,934件の閲覧回数
b36401
NXP Employee
NXP Employee

Possibly UART connection is weak and the connection drops by some glitch.
Please try to change cable, etc.

0 件の賞賛
返信
1,918件の閲覧回数
mt_android
Contributor I

I changed the cable, and it is the samething. The ADB connection gets lost in several minutes after plugged in.

0 件の賞賛
返信