iMX8 Inline Encryption Engine (AES-128).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 Inline Encryption Engine (AES-128).

Jump to solution
5,461 Views
mariusznajmowic
Contributor I

iMX8 has Inline Encryption Engine (AES-128). Do this unit is able to encrypt/decrypt DDR4 contest on the fly ?

1 Solution
5,241 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mariusz

yes it is able to encrypt/decrypt DDR4 contest on the fly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
5,241 Views
mariusznajmowic
Contributor I

Thank You for fast answer. Do anybody now how much encryption slow down access/execution code from DDR4 ?

0 Kudos
Reply
5,241 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mariusz

 

sorry I am not aware of such data, note this part is not publicly released yet

and has limited support.

 

Best regards
igor

0 Kudos
Reply
5,242 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mariusz

yes it is able to encrypt/decrypt DDR4 contest on the fly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------