iMX8 Inline Encryption Engine (AES-128).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 Inline Encryption Engine (AES-128).

ソリューションへジャンプ
5,665件の閲覧回数
mariusznajmowic
Contributor I

iMX8 has Inline Encryption Engine (AES-128). Do this unit is able to encrypt/decrypt DDR4 contest on the fly ?

1 解決策
5,445件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mariusz

yes it is able to encrypt/decrypt DDR4 contest on the fly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
5,445件の閲覧回数
mariusznajmowic
Contributor I

Thank You for fast answer. Do anybody now how much encryption slow down access/execution code from DDR4 ?

0 件の賞賛
返信
5,445件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mariusz

 

sorry I am not aware of such data, note this part is not publicly released yet

and has limited support.

 

Best regards
igor

0 件の賞賛
返信
5,446件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mariusz

yes it is able to encrypt/decrypt DDR4 contest on the fly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------