iMX7D VBUS detection treshold?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX7D VBUS detection treshold?

跳至解决方案
1,311 次查看
thomaskofoedhan
Contributor III

What is the VBUS detection treshold?

It is mentioned several times in the documentation and one can even make adjustments to it in percent, but no mention of the actual value.

Thomas

标签 (1)
0 项奖励
回复
1 解答
1,184 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

please refer to sect.11.4.5.4 USB OTG PHY Configuration Register 2

(USBNC_n_PHY_CFG2) i.MX7D  RM
The VBUS Valid threshold is nominally 4.75V on this USB PHY. 

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,185 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

please refer to sect.11.4.5.4 USB OTG PHY Configuration Register 2

(USBNC_n_PHY_CFG2) i.MX7D  RM
The VBUS Valid threshold is nominally 4.75V on this USB PHY. 

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复