iMX7D VBUS detection treshold?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7D VBUS detection treshold?

Jump to solution
1,848 Views
thomaskofoedhan
Contributor III

What is the VBUS detection treshold?

It is mentioned several times in the documentation and one can even make adjustments to it in percent, but no mention of the actual value.

Thomas

Labels (1)
0 Kudos
Reply
1 Solution
1,721 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

please refer to sect.11.4.5.4 USB OTG PHY Configuration Register 2

(USBNC_n_PHY_CFG2) i.MX7D  RM
The VBUS Valid threshold is nominally 4.75V on this USB PHY. 

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,722 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

please refer to sect.11.4.5.4 USB OTG PHY Configuration Register 2

(USBNC_n_PHY_CFG2) i.MX7D  RM
The VBUS Valid threshold is nominally 4.75V on this USB PHY. 

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply