iMX7D VBUS detection treshold?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7D VBUS detection treshold?

ソリューションへジャンプ
1,857件の閲覧回数
thomaskofoedhan
Contributor III

What is the VBUS detection treshold?

It is mentioned several times in the documentation and one can even make adjustments to it in percent, but no mention of the actual value.

Thomas

ラベル(1)
0 件の賞賛
返信
1 解決策
1,730件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

please refer to sect.11.4.5.4 USB OTG PHY Configuration Register 2

(USBNC_n_PHY_CFG2) i.MX7D  RM
The VBUS Valid threshold is nominally 4.75V on this USB PHY. 

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,731件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

please refer to sect.11.4.5.4 USB OTG PHY Configuration Register 2

(USBNC_n_PHY_CFG2) i.MX7D  RM
The VBUS Valid threshold is nominally 4.75V on this USB PHY. 

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信