iMX7D : SAI (Serial Audio Interface)Timing Parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7D : SAI (Serial Audio Interface)Timing Parameters

ソリューションへジャンプ
5,211件の閲覧回数
koichisakagami
Contributor II

Dear community,
We have been developing our product with iMX7D.

I am checking a Serial Audio Interface.


I hope to get a  SAI (Serial Audio Interface)Timing Parameters .
But I could not find the  SAI Timing Parameters description in Data Sheet IMX7DCEC Rev2 .

[Question]
        Could you tell me the SAI Timing Parameters specification ?

Best Regards,
       Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
4,901件の閲覧回数
art
NXP Employee
NXP Employee

Unfortunately, the SAI section is not included in the current revision of the i.MX7D Data Sheet document, will be fixed in further releases.

The SAI module is compliant with the I2S specification by Philips (see attached) and AC97 rev.2.3 specification by Intel:

http://download.intel.com/support/motherboards/desktop/sb/ac97_r23.pdf

So, the basic timings are as defined in the corresponding specifications.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,901件の閲覧回数
koichisakagami
Contributor II

Dear Artur san,
Thank you for your information.

Do you have a Data Sheet schedule in which the SAI timing specification is described ?

Best Regards,

       Koichi Sakagami

0 件の賞賛
返信
4,901件の閲覧回数
art
NXP Employee
NXP Employee

Sorry, no exact schedule is available yet. I'm opening the ticket for the documentation team regarding the issue you've found.

Best Regards,

Artur

0 件の賞賛
返信
4,902件の閲覧回数
art
NXP Employee
NXP Employee

Unfortunately, the SAI section is not included in the current revision of the i.MX7D Data Sheet document, will be fixed in further releases.

The SAI module is compliant with the I2S specification by Philips (see attached) and AC97 rev.2.3 specification by Intel:

http://download.intel.com/support/motherboards/desktop/sb/ac97_r23.pdf

So, the basic timings are as defined in the corresponding specifications.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,901件の閲覧回数
mike_susen
NXP Employee
NXP Employee
0 件の賞賛
返信