iMX7 support of PCM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX7 support of PCM

1,569 次查看
awong121
Contributor I

I want to know whether iMX7 Dual can support PCM from one of the SAI ports. I was told that in iMX6 it is possible, but I have not seen any mention of PCM in iMX7 in the reference manual, Thanks.

标签 (1)
0 项奖励
回复
2 回复数

1,361 次查看
BiyongSUN
NXP Employee
NXP Employee

In the reference manual.  It is very clear you can configure the SYWD FSE for PCM A and PCM B and I2S.

Untitled.png

0 项奖励
回复

1,361 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andy

yes it supports, as PCM is generic name for many formats

in particular SAI supports TDM

Pulse-code modulation - Wikipedia, the free encyclopedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复