iMX7 support of PCM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7 support of PCM

1,615 Views
awong121
Contributor I

I want to know whether iMX7 Dual can support PCM from one of the SAI ports. I was told that in iMX6 it is possible, but I have not seen any mention of PCM in iMX7 in the reference manual, Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,407 Views
BiyongSUN
NXP Employee
NXP Employee

In the reference manual.  It is very clear you can configure the SYWD FSE for PCM A and PCM B and I2S.

Untitled.png

0 Kudos
Reply

1,407 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andy

yes it supports, as PCM is generic name for many formats

in particular SAI supports TDM

Pulse-code modulation - Wikipedia, the free encyclopedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply