iMX6UL - DDR ADDR drive strength read-only

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL - DDR ADDR drive strength read-only

ソリューションへジャンプ
1,468件の閲覧回数
nickbedbury
Contributor III

For the iMX6UL, why is the drive strength (DSE) setting for DDR ADDRn pins in IOMUX read-only?

For example, see the IOMUXC_SW_PAD_CTL_PAD_DRAM_ADDR00 section of the reference manual:

pastedImage_1.png

I would have expected the DSE bitfield to have a variety of configurable options, since ADDR is an output of the iMX6...  But instead DSE is disabled and read-only.

ラベル(1)
タグ(2)
1 解決策
1,372件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

these settings are configured by SW_PAD_CTL_GRP_ADDDS SW GRP Register
(IOMUXC_SW_PAD_CTL_GRP_ADDDS), described in sect.30.5.288 i.MX6UL

Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,373件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

these settings are configured by SW_PAD_CTL_GRP_ADDDS SW GRP Register
(IOMUXC_SW_PAD_CTL_GRP_ADDDS), described in sect.30.5.288 i.MX6UL

Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,372件の閲覧回数
nickbedbury
Contributor III

Thanks, I was not aware of that register

0 件の賞賛
返信