iMX6SL cannot boot from eMMC when LCD is connected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SL cannot boot from eMMC when LCD is connected

1,376 Views
namratanalawade
Contributor I

Hi,

We have a cutom board based on IMX6SL EVK. Board boots when LCD is not connected to it. But we are facing an issue that board is not booting from eMMC when LCD is connected. 

We also referred i.MX6UL cannot boot from eMMC when LCD is connected this link but still there is an issue.

as per above link there is a comment to disconnect LCD data lines DATA4 to DATA13 but we cannot disconnect LCD data lines. Also we have measured the POR_B voltage.

Any help to resolve this issue.

Thanks in advance

0 Kudos
Reply
1 Reply

1,314 Views
igorpadykov
NXP Employee
NXP Employee

Hi  Namrata

please attach jtag and check SRC_SBMR1,2 registers if they have
correct boot configuration.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply