iMX6SL cannot boot from eMMC when LCD is connected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6SL cannot boot from eMMC when LCD is connected

1,351件の閲覧回数
namratanalawade
Contributor I

Hi,

We have a cutom board based on IMX6SL EVK. Board boots when LCD is not connected to it. But we are facing an issue that board is not booting from eMMC when LCD is connected. 

We also referred i.MX6UL cannot boot from eMMC when LCD is connected this link but still there is an issue.

as per above link there is a comment to disconnect LCD data lines DATA4 to DATA13 but we cannot disconnect LCD data lines. Also we have measured the POR_B voltage.

Any help to resolve this issue.

Thanks in advance

0 件の賞賛
返信
1 返信

1,289件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi  Namrata

please attach jtag and check SRC_SBMR1,2 registers if they have
correct boot configuration.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信