iMX6SL BT.656 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SL BT.656 interface

Jump to solution
2,545 Views
James_wang
Contributor I

Hi

The iMX6SL RM Page 786 shows the eLCDIF support ITU-R BT.656 Digital Video Interface. Anyone have idea whether the android driver is available? Does the chipset and driver support hot switch between MPU interface and BT656 interface?

Thanks.

Labels (3)
0 Kudos
Reply
1 Solution
1,896 Views
lily_zhang
NXP Employee
NXP Employee

Because there is no device with BT656 support connected to MX6SL EVK board, no BSP driver is ready for BT656 support. You can refer to "21.2.9 ITU-R BT.656 Digital Video Interface (DVI)" to know the basic flow for register setting when enabling BT.656 mode.

View solution in original post

0 Kudos
Reply
1 Reply
1,897 Views
lily_zhang
NXP Employee
NXP Employee

Because there is no device with BT656 support connected to MX6SL EVK board, no BSP driver is ready for BT656 support. You can refer to "21.2.9 ITU-R BT.656 Digital Video Interface (DVI)" to know the basic flow for register setting when enabling BT.656 mode.

0 Kudos
Reply