iMX6SL BT.656 interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6SL BT.656 interface

跳至解决方案
2,638 次查看
James_wang
Contributor I

Hi

The iMX6SL RM Page 786 shows the eLCDIF support ITU-R BT.656 Digital Video Interface. Anyone have idea whether the android driver is available? Does the chipset and driver support hot switch between MPU interface and BT656 interface?

Thanks.

标签 (3)
标记 (4)
0 项奖励
回复
1 解答
1,989 次查看
lily_zhang
NXP Employee
NXP Employee

Because there is no device with BT656 support connected to MX6SL EVK board, no BSP driver is ready for BT656 support. You can refer to "21.2.9 ITU-R BT.656 Digital Video Interface (DVI)" to know the basic flow for register setting when enabling BT.656 mode.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,990 次查看
lily_zhang
NXP Employee
NXP Employee

Because there is no device with BT656 support connected to MX6SL EVK board, no BSP driver is ready for BT656 support. You can refer to "21.2.9 ITU-R BT.656 Digital Video Interface (DVI)" to know the basic flow for register setting when enabling BT.656 mode.

0 项奖励
回复