iMX6SL BT.656 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6SL BT.656 interface

ソリューションへジャンプ
2,572件の閲覧回数
James_wang
Contributor I

Hi

The iMX6SL RM Page 786 shows the eLCDIF support ITU-R BT.656 Digital Video Interface. Anyone have idea whether the android driver is available? Does the chipset and driver support hot switch between MPU interface and BT656 interface?

Thanks.

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
1,923件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Because there is no device with BT656 support connected to MX6SL EVK board, no BSP driver is ready for BT656 support. You can refer to "21.2.9 ITU-R BT.656 Digital Video Interface (DVI)" to know the basic flow for register setting when enabling BT.656 mode.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,924件の閲覧回数
lily_zhang
NXP Employee
NXP Employee

Because there is no device with BT656 support connected to MX6SL EVK board, no BSP driver is ready for BT656 support. You can refer to "21.2.9 ITU-R BT.656 Digital Video Interface (DVI)" to know the basic flow for register setting when enabling BT.656 mode.

0 件の賞賛
返信