iMX6 trace clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 trace clock

1,348 Views
lucaellero
Contributor I

Hi,

I'm using a Lauterbach debugger/trace on a iMX6 platform.

For an efficient tracing I would like to increase the trace clock, now it is set to 66 MHz. Optimum frequency would be something around 200 MHz..

Can someone kindly suggest me how to do that, the iMX6 Reference Manual doesn't help in this case.

Thank you

Regards

Luca

Labels (1)
0 Kudos
Reply
2 Replies

1,201 Views
Yuri
NXP Employee
NXP Employee

"The Trace clocks are derived directly from the AHB clock. There is no ability

to change the trace clock frequencies other than changing the AHB clock

frequency, which will have multiple side effects in the system. So essentially,

no you cannot change the Trace clock frequency."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,201 Views
lucaellero
Contributor I

Hi Yuri,

thank you for your kind reply.

regards

Luca

0 Kudos
Reply