iMX6 trace clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 trace clock

1,886件の閲覧回数
lucaellero
Contributor I

Hi,

I'm using a Lauterbach debugger/trace on a iMX6 platform.

For an efficient tracing I would like to increase the trace clock, now it is set to 66 MHz. Optimum frequency would be something around 200 MHz..

Can someone kindly suggest me how to do that, the iMX6 Reference Manual doesn't help in this case.

Thank you

Regards

Luca

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,739件の閲覧回数
Yuri
NXP Employee
NXP Employee

"The Trace clocks are derived directly from the AHB clock. There is no ability

to change the trace clock frequencies other than changing the AHB clock

frequency, which will have multiple side effects in the system. So essentially,

no you cannot change the Trace clock frequency."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,739件の閲覧回数
lucaellero
Contributor I

Hi Yuri,

thank you for your kind reply.

regards

Luca

0 件の賞賛
返信