iMX6 integrated LDO's

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 integrated LDO's

ソリューションへジャンプ
2,306件の閲覧回数
tarterkit_ru
Contributor III

If chip marked as 1GHz ability, how up frequency in Linux kernel to 1G?

As i understand, if put cpu_freq=1G to kernel komand line arguments, it is disable integrated LDO's and must be supply external МСС to ARM_CAP ...

ラベル(2)
0 件の賞賛
返信
1 解決策
1,727件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

According to the Linux BSP Release Note, you can put the "arm_freq=1000" in the kernel command line. Basically,

1G CPU frequency is set by default and LDO bypass is enabled by default.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,728件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

According to the Linux BSP Release Note, you can put the "arm_freq=1000" in the kernel command line. Basically,

1G CPU frequency is set by default and LDO bypass is enabled by default.

0 件の賞賛
返信