iMX6 UART time between bytes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 UART time between bytes

ソリューションへジャンプ
1,574件の閲覧回数
joseluiszabalz1
Contributor II

Is it possible configure the time between bytes in a iMX6 UART?

I could no find a register in iMX6 UART to define the time between bytes when the UART TxFifo is filled out.

Is it defined by SOC hardware?

Thanks in advance.

ラベル(1)
1 解決策
1,520件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jose

you are right, it is defined by SOC hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,521件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jose

you are right, it is defined by SOC hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------