iMX6 UART time between bytes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 UART time between bytes

跳至解决方案
981 次查看
joseluiszabalz1
Contributor II

Is it possible configure the time between bytes in a iMX6 UART?

I could no find a register in iMX6 UART to define the time between bytes when the UART TxFifo is filled out.

Is it defined by SOC hardware?

Thanks in advance.

标签 (1)
1 解答
927 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jose

you are right, it is defined by SOC hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
928 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jose

you are right, it is defined by SOC hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------