iMX6 UART time between bytes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 UART time between bytes

Jump to solution
1,580 Views
joseluiszabalz1
Contributor II

Is it possible configure the time between bytes in a iMX6 UART?

I could no find a register in iMX6 UART to define the time between bytes when the UART TxFifo is filled out.

Is it defined by SOC hardware?

Thanks in advance.

Labels (1)
1 Solution
1,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

you are right, it is defined by SOC hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,527 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

you are right, it is defined by SOC hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------