iMX6 Quad processor Bring up in Sabre platform for Automotive Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Quad processor Bring up in Sabre platform for Automotive Application

970 Views
dibing
Contributor I

Hi,

I have designed a Vehicle infotainment system using iMX6 quad processor in Sabre platform. iMX6 processor is in CPU board which have no USB port in it. so i can't do the Uboot only with the CPU board.

For the initial test, I am planning to program the SPI boot image to SPI NOR flash externally and place in the CPU board. 

I have downloaded some Uboot files from NXP.com, but did not identified the externally programmable SPI NOR flash image.

Please help me by providing the SPI NOR flsh image or by telling how can i get that file.

regards, 

0 Kudos
Reply
1 Reply

901 Views
joanxie
NXP TechSupport
NXP TechSupport

one can refer to the link as below, one can check if your hardware is correct or not.

https://community.nxp.com/thread/311437#comment-347573 

0 Kudos
Reply