iMX28 Linux Device Tree - Configure Pin for External Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 Linux Device Tree - Configure Pin for External Interrupt

5,789 Views
rabryn
Contributor III

Can anyone help me define a device tree node that configures a GPIO pin to generate an interrupt?  I have a device that asserts an IRQ and would like to handle it in the kernel.  I'm attempting to use MX28_PAD_GPMI_D04__GPIO_0_4 for the IRQ pin.  I'm also using a mainline 3.8.3 kernel.

Thanks,

Ryan

0 Kudos
Reply
3 Replies

3,478 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Ryan,

I haven't tried it on mx28, but on mx5 we have an example for GPIO interrupt in imx51-babbage.dts:

https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/arch/arm/boot/dts/imx51-ba...

Please check the PMIC node, that has a GPIO that triggers an interrupt.

If you still face issues, please post this question into the linux-arm-kernel  mailing list.

Regards,

Fabio Estevam

3,478 Views
rabryn
Contributor III

Fabio,

Thanks for the response.  I've seen that in the imx51-babbage.dts file, but I'm still confused.  In the kernel source, under Documentation/devicetree/bindings/gpio, I see the following in gpio-mxs.txt:

As the GPIO controller is embedded in the PIN controller and all the

GPIO ports share the same IO space with PIN controller, the GPIO node

will be represented as sub-nodes of MXS pinctrl node.

Required properties for GPIO node:

- compatible : Should be "fsl,<soc>-gpio".  The supported SoCs include

  imx23 and imx28.

- interrupts : Should be the port interrupt shared by all 32 pins.

- gpio-controller : Marks the device node as a gpio controller.

- #gpio-cells : Should be two.  The first cell is the pin number and

  the second cell is used to specify the gpio polarity:

      0 = active high

      1 = active low

- interrupt-controller: Marks the device node as an interrupt controller.

- #interrupt-cells : Should be 2.  The first cell is the GPIO number.

  The second cell bits[3:0] is used to specify trigger type and level flags:

      1 = low-to-high edge triggered.

      2 = high-to-low edge triggered.

      4 = active high level-sensitive.

      8 = active low level-sensitive.

Note: Each GPIO port should have an alias correctly numbered in "aliases"

node.

Then in the imx28.dtsi I see the definitions of the aliases and GPIO ports, for example...

                gpio0: gpio@0 {

                    compatible = "fsl,imx28-gpio", "fsl,mxs-gpio";

                    interrupts = <127>;

                    gpio-controller;

                    #gpio-cells = <2>;

                    interrupt-controller;

                    #interrupt-cells = <2>;

                };

I don't see how I should define a node in the imx28-evk.dts that defines a GPIO that is an IRQ.  The "interrupts" in the dtsi file, 127 in the example above, refer to the IRQ source in the ICOLL.  Where are the definitions of the interrupt-cells and gpio-cells at that are described in the gpio-mxs.txt documentation?

Thanks,

Ryan

0 Kudos
Reply

3,478 Views
fabio_estevam
NXP Employee
NXP Employee

I am not sure. Please start a thread in linux-arm-kernel mailing list.

Regards,

Fabio Estevam

0 Kudos
Reply