iMX Yocto: Adding ffmpeg & mongoose to iMX6 image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX Yocto: Adding ffmpeg & mongoose to iMX6 image

4,159 次查看
tejasshah
Contributor III

Hello,

I am trying to create an image using yocto for iMX6 sololite board and want to include ffmpeg & mongoose in my image.

I added ffmpeg & mongoose in conf/local.conf by using IMAGE_INSTALL_append but while it is running, it keeps on

giving me an error that:

ERROR: Nothing PROVIDES 'ffmpeg'

ERROR: Nothing PROVIDES 'mongoose'

I need help in getting these two packages in my final image.

I have installed gst-ffmpeg in my image. Is it possible to use gst-ffmpeg in place of ffmpeg to segment a .mp4 file into .ts file segments (HLS segments)?

I looked up on google to find examples related to using gst-ffmpeg, but I wasn't successful.

It is very urgent.

标记 (1)
0 项奖励
回复
4 回复数

1,875 次查看
tejasshah
Contributor III

I posted the above message before 4 days, but no one is replying.

Please reply, it is very urgent :smileysad:.

0 项奖励
回复

1,875 次查看
LeonardoSandova
Specialist I

Hi Tejas, my suggestion is to post this into the meta-freescale list (in case you have not...)

Leo

0 项奖励
回复

1,875 次查看
tejasshah
Contributor III

How can I do that?

I tried to move the post but didn't find meta-freescale option in there for moving it.

0 项奖励
回复

1,875 次查看
LeonardoSandova
Specialist I
0 项奖励
回复