IMX6Q - TVP5150 Support - BT656

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q - TVP5150 Support - BT656

Jump to solution
2,326 Views
patrickmccleary
Contributor II

Hello Everybody.

My first post on the i.MX Community forum! Anyway, I'm trying to incorporate a composite video input into the IMX6Q using TI's TVP5150 (BT656 NTSC) through the parallel camera interface (CSI0). I've got the TVP5150 kernel driver talking to the chip through the i2c bus but I'm not sure how to register it with v4l2. I'm pretty new to the linux kernel and v4l2 so any help or information would be greatly appreciated. Thanks!

I've also attached my board schematic to this post. If anyone would like the gerbers let me know.

-Pat

Labels (4)
Tags (2)
0 Kudos
1 Solution
938 Views
patrickmccleary
Contributor II

Hello Jimmy. My solution is to use the ADV7180 instead of the TVP5150AM1 as the FSL specific v4l2 kernel drivers support it out of the box.

View solution in original post

0 Kudos
2 Replies
938 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think you can read the linux BSP porting guide for more information about porting a camera/video input.

The document is i.MX_6Dual6Quad_BSP_Porting_Guide.pdf in the Linux BSP bundle.

you can download it from here:

i.MX 6 Series Software and Development Tool Resources Product Summary Page

0 Kudos
939 Views
patrickmccleary
Contributor II

Hello Jimmy. My solution is to use the ADV7180 instead of the TVP5150AM1 as the FSL specific v4l2 kernel drivers support it out of the box.

0 Kudos