i.mx6sl support for RMII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6sl support for RMII

Jump to solution
2,645 Views
kentmeyer
Contributor II

For backward compatibility reasons, we are trying to figure out if the i.mx6sl supports RMII.

If so, can you point us at documentation, or describe the pins/signals supporting it?

Hopefully others have had this similar question and have an answer.

Many Thanks!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,350 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kent

yes it supports, please refer below

Re: iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

RMII on i.MX6 (L3.0.35_4.1.0)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,351 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kent

yes it supports, please refer below

Re: iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

RMII on i.MX6 (L3.0.35_4.1.0)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,350 Views
kentmeyer
Contributor II

Thanks Igor!

-- Kent

0 Kudos
Reply