i.mx6sl support for RMII

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6sl support for RMII

跳至解决方案
1,744 次查看
kentmeyer
Contributor II

For backward compatibility reasons, we are trying to figure out if the i.mx6sl supports RMII.

If so, can you point us at documentation, or describe the pins/signals supporting it?

Hopefully others have had this similar question and have an answer.

Many Thanks!

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,449 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kent

yes it supports, please refer below

Re: iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

RMII on i.MX6 (L3.0.35_4.1.0)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,450 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kent

yes it supports, please refer below

Re: iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

RMII on i.MX6 (L3.0.35_4.1.0)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,449 次查看
kentmeyer
Contributor II

Thanks Igor!

-- Kent

0 项奖励
回复