i.mx6 solo主芯片,是否支持Trustzone?如果支持安全存储功能,需要做哪些工作?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 solo主芯片,是否支持Trustzone?如果支持安全存储功能,需要做哪些工作?

1,263 Views
yongheluo_hotma
Contributor III

Dear Sir,

    敝司使用的主芯片为i.mx6 solo单核芯片,不知这颗芯片是否能支持Trustzone。

    如果支持的话,要使用Trustzone功能,需要做哪些工作?如:开启Secure boot?使用哪个Trustzone的OS(ex. OP-TEE)?使用有具体的Porting文档?

   另外,敝司设备主要目的是要实现SecureBoot和安全存储的要求。除了采用Trustzone技术之外,好像还有SNVS(Secure Non-Volatile Storage)等策略,可以实现安全存储的目的?

   请问,是否有相关的建议和文档,以期能够实现项目所要求的功能。

    谢谢!

   罗永和

Labels (1)
0 Kudos
Reply
1 Reply

1,027 Views
b36401
NXP Employee
NXP Employee

What you need is i.MX6 Security Reference Manual that you can request on Reference Manual tab on i.MX6S Documentation page:

i.MX 6Solo Applications Processors | Single Arm® Cortex®-A9 @ 1GHz |NXP 

Please note that your NXP sales person or FAE sould approve download request.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply