i.mx6 DualLite processor parallel Display RGB ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 DualLite processor parallel Display RGB ports

ソリューションへジャンプ
2,078件の閲覧回数
prev
Contributor II

Hi,

Reg Display Parallel port RGB pins.

As per Sabre lite EVM schematics, the Parallel ports RGB pins are connected as follows

Which port are R,G, B.?

is it this way as shown below,

DISP0_DAT [0-7]  is Blue

DISP0_DAT[8-15] is Green

DISP0_DAT[16-23] is Red

Is this configuration correct, am not able to find the processor datasheet  file name IMX6SDLRM.pdf

Can you Confirm.

pastedImage_0.png

pastedImage_1.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,741件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prev

please check sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6SDL Datasheet (rev.4, 12/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

and sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,742件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prev

please check sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6SDL Datasheet (rev.4, 12/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

and sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信