i.mx6 DualLite processor parallel Display RGB ports

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 DualLite processor parallel Display RGB ports

Jump to solution
2,098 Views
prev
Contributor II

Hi,

Reg Display Parallel port RGB pins.

As per Sabre lite EVM schematics, the Parallel ports RGB pins are connected as follows

Which port are R,G, B.?

is it this way as shown below,

DISP0_DAT [0-7]  is Blue

DISP0_DAT[8-15] is Green

DISP0_DAT[16-23] is Red

Is this configuration correct, am not able to find the processor datasheet  file name IMX6SDLRM.pdf

Can you Confirm.

pastedImage_0.png

pastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Solution
1,761 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prev

please check sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6SDL Datasheet (rev.4, 12/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

and sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,762 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prev

please check sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6SDL Datasheet (rev.4, 12/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

and sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply