i.mx6 DualLite processor parallel Display RGB ports

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.mx6 DualLite processor parallel Display RGB ports

跳至解决方案
2,097 次查看
prev
Contributor II

Hi,

Reg Display Parallel port RGB pins.

As per Sabre lite EVM schematics, the Parallel ports RGB pins are connected as follows

Which port are R,G, B.?

is it this way as shown below,

DISP0_DAT [0-7]  is Blue

DISP0_DAT[8-15] is Green

DISP0_DAT[16-23] is Red

Is this configuration correct, am not able to find the processor datasheet  file name IMX6SDLRM.pdf

Can you Confirm.

pastedImage_0.png

pastedImage_1.png

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,760 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prev

please check sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6SDL Datasheet (rev.4, 12/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

and sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,761 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prev

please check sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6SDL Datasheet (rev.4, 12/2014)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

and sect.4.11.10.4 IPU Display Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复