i.mx6 CSI0_DATA_EN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,691件の閲覧回数
allanmatthew
Contributor IV

Is there a diagram anywhere of the timing required when using the CSI0_DATA_EN pin?  The Reference Manual and i.MX6 datasheets do not show the pin in any diagram or description that I've seen. 

Furthermore, is there any configuration required to enable the DATA_ENABLE pin beyond setting it in the DTB (pinctl_ipu1_2) and setting the csi_param.data_en_pol?

Thanks

0 件の賞賛
返信
1 解決策
3,306件の閲覧回数
allanmatthew
Contributor IV

For anyone else struggling with this, I received this diagram from FSL support:

Screen Shot 2014-08-29 at 7.14.52 AM.png

Screen Shot 2014-08-29 at 7.15.18 AM.png

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,307件の閲覧回数
allanmatthew
Contributor IV

For anyone else struggling with this, I received this diagram from FSL support:

Screen Shot 2014-08-29 at 7.14.52 AM.png

Screen Shot 2014-08-29 at 7.15.18 AM.png

0 件の賞賛
返信
3,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Allan

I am afraid such diagram is not available.

Answer on second qustion is no, in Freescale BSPs this DATA_ENABLE

signal is just set to correct value, so CSI could accept data.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,306件の閲覧回数
allanmatthew
Contributor IV

Chip- should the DE be active-high or active-low?

0 件の賞賛
返信
3,306件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

DE is active-high

Best regards

chip

0 件の賞賛
返信