i.mx6 CSI0_DATA_EN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6 CSI0_DATA_EN

Jump to solution
2,801 Views
allanmatthew
Contributor IV

Is there a diagram anywhere of the timing required when using the CSI0_DATA_EN pin?  The Reference Manual and i.MX6 datasheets do not show the pin in any diagram or description that I've seen. 

Furthermore, is there any configuration required to enable the DATA_ENABLE pin beyond setting it in the DTB (pinctl_ipu1_2) and setting the csi_param.data_en_pol?

Thanks

0 Kudos
Reply
1 Solution
2,416 Views
allanmatthew
Contributor IV

For anyone else struggling with this, I received this diagram from FSL support:

Screen Shot 2014-08-29 at 7.14.52 AM.png

Screen Shot 2014-08-29 at 7.15.18 AM.png

View solution in original post

0 Kudos
Reply
4 Replies
2,417 Views
allanmatthew
Contributor IV

For anyone else struggling with this, I received this diagram from FSL support:

Screen Shot 2014-08-29 at 7.14.52 AM.png

Screen Shot 2014-08-29 at 7.15.18 AM.png

0 Kudos
Reply
2,416 Views
igorpadykov
NXP Employee
NXP Employee

Hi Allan

I am afraid such diagram is not available.

Answer on second qustion is no, in Freescale BSPs this DATA_ENABLE

signal is just set to correct value, so CSI could accept data.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,416 Views
allanmatthew
Contributor IV

Chip- should the DE be active-high or active-low?

0 Kudos
Reply
2,416 Views
igorpadykov
NXP Employee
NXP Employee

DE is active-high

Best regards

chip

0 Kudos
Reply