i.Mx6 Parallel CSI0 16bit bus width

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.Mx6 Parallel CSI0 16bit bus width

Jump to solution
2,576 Views
alessandroinnoc
Contributor II

Hi to all !

I am interfacing an ADV7403 to iMX6 DUAL using CSI0 port at 16bit bus width, but I also get

I always get the following kernel error message:

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0.

Does anyone have any experience on such interfacing ?

Best Regards

Alessandro Innocenti

Labels (1)
0 Kudos
Reply
1 Solution
2,093 Views
alessandroinnoc
Contributor II

Hi chip

we solved using CSI0 with a bus 8 bit wide and doubling the pixel clock.

Many thanks

ALessandro Innocenti

View solution in original post

0 Kudos
Reply
2 Replies
2,092 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alessandro

seems this configuration is not supported in kernel,

one can look at similar post below

How to fix the camera timeout error ?

In general new camera needs some support code, for

example ADV7180 below

https://community.freescale.com/message/314760#314760

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,094 Views
alessandroinnoc
Contributor II

Hi chip

we solved using CSI0 with a bus 8 bit wide and doubling the pixel clock.

Many thanks

ALessandro Innocenti

0 Kudos
Reply