i.MXRT1064 EVK PCB file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MXRT1064 EVK PCB file

2,153 次查看
msbala
Contributor I

Dear NXP Deam,

Kindly help me on this customer support.

 

We want to study the i.MXRT1064 EVK PCB file which is in Allegro tool.

We want to open it in Altium, for that ASCII file generated from Allegro is required.

Please help to provide that as well.

 

EVK LINK

https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/mimxrt1064-evk-...

Thanks 

Bala

标签 (1)
0 项奖励
回复
5 回复数

1,946 次查看
zulu1877
Contributor I

Dear NXP Team,

 

Im in exactly the same situation,

I use altuim only, could i please get a copy of the files to import please?

  

EVK LINK

https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/mimxrt1064-evk-...

 

Thanks 

Nick

0 项奖励
回复

1,946 次查看
Yuri
NXP Employee
NXP Employee

Hello, zulu1877@gmail.com !

 Is it possible for You to create request ?

Support | NXP 

Regards,

Yuri.

0 项奖励
回复

1,946 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You directly the PCB file, which can be imported in Altium.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复

1,942 次查看
MarkDudley
Contributor I

Yuri would it be possible for me to get these files as well?

0 项奖励
回复

1,930 次查看
Yuri
NXP Employee
NXP Employee

@MarkDudley 
Hello,

   Is it possible for You to create request ?

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

 

~Yuri.

 

0 项奖励
回复